MaximumPackageSize property

Gets or sets the maximum packet size. Read/write. Long.
Syntax
connOption
.
MaximumPackageSize
where
connOption
- is an MQTTConnectOption object created by the MQTTFactory object's method
CreateConnectOption
.
Default value
If this property is omitted, it will use its default value, which is 256 MB. However, resource-constrained clients and some MQTT servers operating as edge gateways may not be able to handle packets of this size.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal