ApplicationMessage event
An event indicating the receipt of application messages. This event will be triggered when the MQTT client receives a message.
Syntax
mqttClient
_ApplicationMessage
(ByVal
eventArgs As
MQTTMessageEvent
)where
mqttClient
- is an MQTTClient object created by the MQTTFactory object's method CreateClient
.Example
Private Sub mqttClient_ApplicationMessage(ByVal msgEvent As MQTTMessageEvent) ' Read message Dim msg As MQTTMessage Set msg = msgEvent.Message Dim msgText As String msgText = msg.PayloadAsText End sub
Provide Feedback