MqttPayloadFormat constants
The payload type of the MQTT message.
MqttPayloadBinary
(0) - Indicates that the payload is unspecified bytes data.MqttPayloadCharacter
(1) - Indicates that the payload is UTF-8 encoded character data.Default value
If no constant is specified, it will use its default value, which is
MqttPayloadBinary
.Provide Feedback