Connect to a broker with WebSocket

Private Sub Connect_WithWebSocket() On Error GoTo errExit Dim connOption As MQTTConnectOption Dim retCode As MqttConnectionCode Set mFactory = Application.CreateMQTT Set mClient = mFactory.CreateClient Set connOption = mFactory.CreateConnectOption() connOption.ClientID = "Client01" connOption.Version = MqttVersion500 connOption.Protocol = MqttProtocolWebSocket connOption.Host = "broker.com" connOption.Port = 8083 connOption.Path = "mqtt" ' It can also be configured directly with the function: ' connOption.WithWebSocketServer "broker.com", 8083, "mqtt" retCode = mClient.Connect(connOption) Exit Sub errExit: MsgBox err.Description End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal