Connect to a broker with TCP
Private Sub Connect_WithTCP() On Error GoTo errExit Dim connOption As MQTTConnectOption Dim retCode As MqttConnectionCode Set mFactory = Application.CreateMQTT Set mClient = mFactory.CreateClient Set connOption = mFactory.CreateConnectOption() connOption.ClientID = "Client01" connOption.Version = MqttVersion500 connOption.Protocol = MqttProtocolTcp connOption.Host = "broker.com" connOption.Port = 1883 ' It can also be configured directly with the function: ' connOption.WithTcpServer "broker.com", 1883 retCode = mClient.Connect(connOption) Exit Sub errExit: MsgBox err.Description End Sub
Provide Feedback