Example: Remove a folder

This example deletes all subfolders within the specified folder. This also deletes all its subfolders and tags.
Sub RemoveFolders(sFolderName As String) On Error GoTo Err_Handler Dim oFolder As Folder Dim oFolders As Folders Set oFolder = TagDB.GetFolder(sFolderName) Set oFolders = oFolder.Folders 'Delete the subfolders in specified folder. Do While oFolders.Count > 0 oFolders.Remove 1 Loop 'Release resources associated with the objects. Set oFolder = Nothing Set oFolders = Nothing Exit Sub Err_Handler: 'Release resources associated with the objects. Set oFolder = Nothing Set oFolders = Nothing MsgBox "Error removing folders." & vbCrLf & vbCrLf & _ Err.Description, vbExclamation, " RemoveFolders" End Sub
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal