Example: Delete a folder
This example deletes the specified folder from the database. All its subfolders and tags are also deleted.
Sub DeleteTagDBFolder(sFolderName As String) On Error GoTo Err_Handler 'Delete the specified folder. TagDB.DeleteFolder sFolderName Exit Sub Err_Handler: MsgBox "Error deleting folder." & vbCrLf & vbCrLf & _ Err.Description, vbExclamation, "DeleteFolder" End Sub
Provide Feedback