gfxServerStatusConstants
The following constants can be returned by the GetServerStatus method.
gfxServerStatusActive
– the server is the active server instancegfxServerStatusStandby
– the server is the standby server instancegfxServerStatusOutOfService
– the server is out of servicegfxServerStatusSecondaryNotDefined
– there is no secondary server defined. Used only for the status of the secondary server.Provide Feedback