gfxServerStateConstants
The following constants can be returned by the GetServerState method.
gfxServerStateActive
(0) – the server is the active servergfxServerStateStandby
(1) – the server is the standby servergfxServerStateOutOfService
(2) – the server is out of service due to failuregfxServerStateSecondaryNotDefined
(3) – the secondary server has not been definedgfxServerStateNotInUse
(4) – the server is out of service through manual interventiongfxServerStateStandbySync
(5) – the server is the standby server and is synchronizing with the active servergfxServerStateActiveSync
(6) – the server is active and is synchronizing with the standby servergfxServerStateActiveNoPartner
(7) – the server is active and disconnected from the standby servergfxServerStateCommError
(8) – Unable to reach hostgfxServerStateLoading
(9) – the server is loadinggfxServerStateStarting
(10) – the server is startinggfxServerStateReady
(11) – the server is ready to provide servicegfxServerStateReadyToBeActive
(12) – the server is synchronized and is ready to become activegfxServerStateReadyToBeStandby
(13) – the server is synchronized and is ready to become standbygfxServerStateNotLoaded
(14) – the server is not loadedProvide Feedback