ftDiagAudienceConstants
Use the ftDiagAudienceConstants to specify the intended audience for a message logged by the LogDiagnosticsMessage method.
ftDiagAudienceRSMACC
(1) – the message is intended for RSMACCftDiagAudienceDeveloper
(2) – the message is intended for technical supportftDiagAudienceEngineer
(4) – the message is intended for control system designers, application engineers, and administratorsftDiagAudienceOperator
(8) – the message is intended for operatorsProvide Feedback