XY Plot template

An template contains a set of settings. A template can be applied to all XY Plots in an HMI server to create a consistent appearance. When you apply a template, the property settings selected for the template are applied to the current XY Plot and will be evident on the runtime chart.
Use an XY Plot template:
  • to apply consistent settings to multiple XY Plot charts.
  • to build a set of different views for the same data.
  • as a quick way to return to a standard display after experimenting with options.
The templates are typically created at runtime and then available for use to all users.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal