Switch between time periods (XY Plot)

For each created time period, a new trace definition is created using the same tags. These additional trace definitions appear in the background of the active trace, so you can compare them.
To switch between time periods
  1. On the
    Time
    bar, click
    Display and Edit All Time Periods
    Trend Linked Icons PNG File Template on the far right to view a list of all time periods. The active time period has a selected radio button to the left of the time period.
  2. Click the radio button beside the time period you want to select.
  3. Click
    Apply
    to save your changes and remain on the list of time periods, or click
    OK
    to save your changes and close the list of time periods.
    TIP:
    Alternate method for switching between time periods:
    On the toolbar, click
    Next Time Period
    Trend Linked Icons PNG File Template to switch between time periods. While you are looking at the trace over one time period, the other trace(s) display in the background of the plot surface.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal