Highlight the active trace (XY Plot)

Highlight the currently selected pair of tags
on the plot surface to make it easier to see when you have multiple tags on the plot surface.
To highlight the active trace
  1. On the
    Trace List
    , select the trace you want to highlight.
  2. On the toolbar, click
    Trace Highlighting
    Trend Linked Icons PNG File Template.
    The trace you selected is highlighted on the plot surface.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal