Layer axes (XY Plot)
Layering the axes is essentially the same as overlaying them, except that the individual axes are automatically displayed and can be dragged to new locations.
To layer the axes
- Right-click the plot surface and clickTag Axes > Layerand select one of the following:
- Y-Axes. If more than one trace exists, displays the y-axis for each trace separately with approximately 10% padding between each.
- X-Axes. If more than one trace exists, displays the x-axis for each trace separately.
- Both. If more than one trace exists, displays the x-axis and y-axis separately.
Provide Feedback