Troubleshooting: Trend chart is missing data when scrolling

Problem
Data outside the visible trend chart area is lost. When you scroll back, or forward, data is missing.
Cause
The trend object stores a limited number of extra data points in addition to those shown. You can set up the amount of extra data stored in a buffer.
Solution
On the
Display
tab in the Trend
Properties
dialog box, set up the
Buffer for Extra Data
option to hold more records per pen.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal