Troubleshooting: Range on trend chart is not as expected
Problem
The range of values shown on a trend chart is not what you expect it to be. For example, the pen's minimum, and maximum values are set up as 1 and 100, but the chart shows a range from -50 to 50.
Cause
The trend object offers a wide variety of range options, controlled by settings on the
Y-Axis
tab. The pen's minimum, and maximum values may fall outside of the specified range, or outside of the specified scale set up on the Y-Axis
tab. It is also possible that the operator has zoomed, or panned along the y-axis.Possible solutions
On the
Y-Axis
tab:- Check whichMinimum / Maximum Valueoption is selected. This option determines how the trend range is set.
- Check whichScale Optionis selected. This option determines the vertical scale for the pens.
- SelectUndo zoom/panfrom the context menu at runtime.
Provide Feedback