Troubleshooting: Numbers display as decimals
Problem
Numbers on the trend chart show as decimals, even though you have selected
Octal
, or Hexadecimal
as the Chart Radix
setting on the Display
tab.Solution
On the
Y-Axis
tab, change the number of decimal places to 0 (zero). If the number of decimal places is set to anything other than zero, numbers cannot be converted accurately to octal, or hexadecimal. To provide accurate data, the trend object shows the numbers as decimals.Provide Feedback