Example: Zoom
Zoom into data by clicking and dragging inside the x-axis, or y-axis scale. You can also click and drag on the chart to zoom into a particular area.
To undo the zoom, right-click and select
Undo Pan/Zoom
.To enable, or disable panning and zooming during runtime, use options on the
Runtime
tab in the Trend Properties
dialog box. The Runtime
tab is not available during runtime.Provide Feedback