Example: Y-axis scale

To include the y-axis legend on a chart, select
Display Scale
on the Y-Axis
tab in the Trend Properties
dialog box.Double-click the y-axis legend at runtime to open the
Y-Axis
tab. This option must be selected on the Runtime
tab.Provide Feedback