Example: Snapshot

Capture and save a snapshot of graphed data and layer that saved data over current data in a trend. This feature allows you to overlay and compare historical data with current data, or any multiple sets of data.
Create a snapshot by using the context menu at runtime.
Add a snapshot to your trend, and set up its overlay options on the
Overlays
tab in the Trend
Properties
dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal