Example: Relocate

tx_relocate
To relocate an overlay's position on a trend chart, right-click the runtime chart, select
Overlays >
Relocate
, and then click the snapshot name. The mouse pointer changes to a two-headed arrow. Click and drag the overlay to position it.
Relocating an overlay changes its offset position.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal