Example: Offset

The offset defines how far a snapshot is anchored from the left edge of a runtime trend chart, in terms of a percentage of the total width of the chart. For example, if you anchor a snapshot by position, and select an offset value of
25%
, the earliest data in the overlay starts at 25 percent of the chart width.Set up offset and overlay options on the
Overlays
tab in the Trend Properties
dialog box.Provide Feedback