Example: Axis legends

tx_AxisLegends
To pan through data, click the y-axis, or x-axis legend and drag the mouse.
To zoom, right-click the horizontal, or vertical axis labels, and drag the mouse.
Show, or hide the axis legends using the
Display Scale
check boxes on the
Y-Axis
, and
X-Axis
tabs in the
Trend Properties
dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal