Options in the Choose Overlay Start Time window
The following table shows the options in the
Choose Overlay Start Time
window.Options | Descriptions |
---|---|
Default Start Time | Click this button if you want to use the default start time specified in the Start date and Start time fields on the X-Axis tab. |
Use Selected Time | Click this button if you want to specify a start time for the overlay instead of using the default. If you select this check box, you must type a time in the Start Time field. |
Start Time | Type the start time for the overlay. This field is available only if the Use Selected Time check box is selected. |
Provide Feedback