TrendPro template
A template contains a set of settings. A template can be applied to all trends in an HMI server to create a consistent appearance. When you apply a template, the property settings selected for the template are applied to the current trend and will be evident on the runtime chart.
Use a trend template:
- to apply consistent settings to multiple trend charts.
- to build a set of different views for the same data.
- as a quick way to return to a standard display after experimenting with options.
The templates are typically created at runtime and then available for use to all users.
Provide Feedback