Layer axes (TrendPro)

Layering the axes is essentially the same as overlaying them, except that the individual axes are automatically displayed and can be dragged to new locations.
To layer the axes
  • Right-click the plot surface and click
    Tag Axes > Layer
    and select one of the following:
    • Y-Axes
      . If more than one trace exists, displays the y-axis for each trace separately with approximately 10% padding between each.
    • X-Axes
      . If more than one time period exists, displays the x-axis for each time period separately.
    • Both
      . If more than one trace and time period exist, displays the x-axis and y-axis separately.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal