Flip axes (TrendPro)
When you flip axes, you determine which side of the plot you want to view the axes on. The axes can be flipped individually – you can flip only the x- or y-axis, or you can flip both axes.
To flip the axes
- Right-click the plot surface, selectTag Axes > Flipand select one of the following:
- Y-Axes. Moves the y-axis to the right side of the plot surface.
- X-Axes. Moves the x-axis to the top of the plot surface.
- Both. Moves the x-axis to the top of the plot surface, and the y-axis to the right side of the plot surface.
Provide Feedback