Time Period page (TrendPro)
How do I open the Time
Period page (Properties dialog box)?
- On thePropertiesdialog box, click theGeneraltab.
- ClickTime Periodin the left pane.
Time period properties allow you to set the update rate for data, determine the time zone to use for data retrieval, and set a relative or absolute time period.
The following properties are applied immediately to the current trend.
TIP:
Each time when TrendPro reads diagnostics from the
FactoryTalk AssetCentre
server, the maximum number of diagnostics is 5,000 for each type of severity.The following options are available:
Options | Description |
---|---|
Period | Determines whether a relative or absolute time period is used. Select one of the following options:
|
Update mode | Determines the method for refreshing data. Select one of the following options:
|
Time zone | Retrieves a data set for a particular time period regardless of the time zone. Select one of the following options:
|
Provide Feedback