Set runtime properties and appearances as default (TrendPro)
TrendPro
general runtime properties and detailed runtime appearances and behaviors can be saved as default in the test run mode on the current computer.
The TrendPro objects you create afterwards will inherit the default properties you configured earlier.
Specifically, these properties include:
- General properties on theGeneraltab of theTrendPro Propertiesdialog box
- Detailed properties on theGeneraltab of thePropertiesdialog box insideTrend Setup:
- Time Period
- Chart
- X-Axis
- Application
- Live Data
- Retrieval
- Shape
- Column settings including column width and which columns to show or hide
- Overall look including layout and which toolbar buttons to show or hide using VBA
To set runtime properties and appearances as default
- After you have configured the runtime properties and appearances in the test run mode, right-click anywhere within the chart, and then selectSet as Default.
Provide Feedback