How inheriting security permissions works in FactoryTalk Security
FactoryTalk Security
FactoryTalk View Studio
Explorer
window.Security permissions on a resource in the Network or Local Directory.
Explorer
window are automatically
inherited from its parent, the object immediately above it in the hierarchy. For example, if
you assign security to an area in an application, the HMI server in the area inherits the
permissions of the area. If you do not explicitly assign security permissions to an area,
the area inherits security settings from the application. The top of the hierarchy is the
FactoryTalk
Basic security access for users and groups at the Network
or Local Directory will be inherited by all resources at lower levels, such applications and
areas. Refine the security for selected users as necessary by overriding inherited
permissions on lower-level resources.
FactoryTalk
The extent to which permissions are inherited depends on how intact the chain of inheritance is. For example, if you select the
Do not inherit permissions
check box for an area, the HMI server within the area can only inherit permissions from the area. It cannot inherit permissions from the application in which the area is located, because the chain of inheritance from the directory at the top of the hierarchy is broken. As breaking the chain of inheritance complicates administration, do so only when it is absolutely necessary.You can also override inherited permissions by assigning explicit permissions, because they take precedence over inherited permissions. For example, if an area inherits permissions from an application, you can override the inherited permissions by specifying permissions explicitly for the users, groups, or computers for the area.
TIP:
- In theFactoryTalk SecuritySettings dialog, inherited permissions are indicated by gray check marks, while explicit permissions are indicated by black check marks.
- For more information about setting upFactoryTalk Securityin FactoryTalk View Site Edition, see Chapter 5 in theFactoryTalk View Site Edition User's Guide, Volume 1.
- For complete details aboutFactoryTalk Security, see theFactoryTalk Services Platform Help.
Provide Feedback