Add users and groups to Runtime Security
After you create users and user groups in FactoryTalk Security, you add them to the security accounts list in the
Runtime Security
editor in FactoryTalk View SE. When you add an account, you also assign the security codes that will give them access to secured HMI components. (Secured HMI components are those that have been assigned security codes.)These codes (A through P), along with those assigned to HMI project components, determine which components a user has access to at runtime. To restrict access to a command, macro, graphic display, OLE object verb, or HMI tag, you assign a security code from A through P to it, and then assign that code only to the users who should have access to the component.
IMPORTANT:
If a user has FactoryTalk View SE runtime security codes assigned to them and FactoryTalk
resources have been secured using FactoryTalk Security, users will need to be given
security permissions in FactoryTalk Security in order to be able to perform actions on a
FactoryTalk View application, such as opening and viewing it in FactoryTalk View Studio,
or writing to a tag at runtime. Security permissions for resources secured at FactoryTalk
Directory are set up in FactoryTalk Security. See the
FactoryTalk Services Platform
Help
for details.For more information about how these features are used in FactoryTalk View, and for
examples of assigning FactoryTalk Security permissions to FactoryTalk View users and user
groups, see Chapter 5 in the
FactoryTalk View Site Edition User's Guide
.Prerequisites
- Add users and groups to FactoryTalk Security
To add users and groups to Runtime Security:
- InFactoryTalk View Studio, clickSettings> Runtime Security.
- In theRuntime Securitydialog box, clickSecurity Accounts.
- In theSecurity Settingsdialog box, in thePermissionstab, clickAdd. This opens theSelect User and Computerdialog box if you are working with a network distributed application, or theSelect User or Groupdialog box if you are working with a local station application.TIP:A local station application has all its components on one computer and so there is no need to specify a computer for the users or groups.
- In theSelect User and Computerdialog box (or theSelect User or Groupdialog box if it is a local station application), below theUserslist, selectShow all, to display the list of all users.TIP:For a network distributed application, below theComputerslist, the default is for theAll Computersto be selected.
- In theUserslist, click the name of a user or group and then clickOK.
- In theSecurity Settingsdialog box, in thePermissionstab, the user you added is selected in theView permissions bysection of the tab.
- To remove security code assignments that do not apply to the user, clear theAllowcheck box beside the relevant codes, and then clickOK. By default, all FactoryTalk View SE security codes are assigned to a new user account.
- In theRuntime Securitydialog box, select the user or group you have just added, and then specify a login and logout macro, if necessary.
Provide Feedback