Scripts editor

How do I open the Scripts editor?
  • In FactoryTalk View Studio, under your application, double-click
    Scripts
    .
Use the
Scripts
editor to create, import, or export a script file. Open the script files and edit them with a script editor, such as PowerShell ISE or other editing program. To set up the default script editor, specify the default program for each type of script file on your operating system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal