Display undefined text strings in the default language

At runtime, if a text string is undefined for the language an application is currently running in, it is displayed as a single question mark (?), unless you have specified that undefined strings are to be displayed using strings from the application's default language.
To display undefined text strings:
  • In the
    Language Configuration
    dialog box, select
    Display undefined strings using the default language
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal