System menu
The System menu commands let you restore, move, size, minimize, maximize, and close the active window, or switch to another window.
To display the System menu for the current window click the box in the left corner of the window's title bar. To close the selected window, double-click the System menu button (the square box in the left corner of a window's title bar).
In the Properties tab of the Display Settings dialog box, you can check or clear the System Menu property to enable or disable it when the display is opened in the FactoryTalk View SE Client.
Provide Feedback