Object key
A key that has had its original action replaced by a command or macro. Object keys are set up in the Graphics editor on a per object basis. When the object has input focus, the keys or mouse buttons assigned to it are available. The operator presses a key or mouse button to carry out the command or macro associated with it.
Provide Feedback