Event

Consists of an expression and an action. The expression is an equation containing tag names, mathematical operators, if-then-else logic, and built-in functions. An action is a FactoryTalk View SE command or macro. Whenever an expression changes from false to true, the action is performed. Set up in the Events editor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal