Client key
A key that has had its original action replaced by a command or macro. Client keys are set up in the Client Keys editor on a per client basis. A client key is available at runtime on a particular FactoryTalk View SE Client, as opposed to display keys (which are active only when a display is active) or object keys (which are active only when an object is selected on a graphic display).
You can specify an initial client key file in the FactoryTalk View SE Client wizard when you create or edit a client.
Provide Feedback