Modify OPC data server properties
Modify the properties of an OPC data server to change settings for tag transfer and events.
To modify the OPC data server properties:
- In the Explorer window, right-click the name of the OPC data server, and then clickProperties.
- In theOPC Data Server Propertiestabs, change the information as required, and then clickOK.
Provide Feedback