HMI Server Properties - Components tab
The following table shows settings in this tab.
Settings | Description |
---|---|
On startup components | For startup components to be loaded and run when the system initializes, the startup type must be set in the HMI Properties General tab to Load and run startup components when operating system initializes .
|
On shutdown macro | Check this option and select a macro that is to be run when the Stop All Running Components button is pressed. |
On active macro | Check this option and select a macro to be run when the server becomes active. This option is only available when redundancy has been set up in the Redundancy tab of the HMI Server Properties dialog box. |
On standby macro | Check this option and select a macro to be run when the server goes into standby mode. This option is only available when redundancy has been set up in the Redundancy tab. |
Run Startup Components | Click this button to manually start all the startup components on the primary server. Note: If the primary HMI server is the active HMI Server and the "Stop all running components" button has been clicked, the "On active" macro will not execute when "Run Startup Components" of the primary HMI server is clicked. This is because the primary HMI Server remained the active HMI Server and never transitioned to the standby HMI Server. |
Stop All Running Components | Click this button to manually stop all components that are running on the primary server including all data log models, all derived tag files and all event files. If a shutdown macro has been specified, it will be run. |
Run Startup Components | Click this button to manually start all the startup components on the secondary server. This option is only available when redundancy has been set up. |
Stop All Running Components | Click this button to manually stop all components that are running on the secondary server including all data log models, all derived tag files and all event files. If a shutdown macro has been specified, it will be run. This option is only available when redundancy has been set up. |
Provide Feedback