Use the Command Wizard
The Command Wizard helps you build command strings by providing lists to choose the commands from, and displaying the syntax for the command. If the command requires parameters, there is a second dialog for selecting parameters and entering additional information. The Command wizard is available anywhere you can enter a FactoryTalk View command.
To build a command string using the Command Wizard:
- InFactoryTalk View Studio, open theCommand Wizard.
- In theCommand Categorieslist, click the folder containing the command you intend to use.
- Click the command. The syntax for it is displayed below the two lists.
- If the command requires parameters, clickNextto go to the second step.
- Specify the parameters the command requires.
- Type or select additional information, as indicated in Step 2 of theCommand Wzard. As you specify parameters, they are added to the command string that is displayed below the parameters.
- ClickFinishwhen the command is complete.
Provide Feedback