Remark

Sends a text string to the Diagnostics system.
This allows operators to send messages to destinations in the Diagnostics system. The severity of the message is set to Information and the audience is set to Operator.
Syntax
Remark <
comment
>
where
<comment>
is a text string up to 132 characters long. The string can contain any characters, including spaces.
Remarks
Enclose the semi-colon (
;
) in single or double quotes, and the apostrophe (
'
) in double quotes.
This command is run locally on the HMI server,
FactoryTalk View SE
Client, or
FactoryTalk View Studio
that issued it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal