PrintDisplay
Prints the specified graphic display to the default printer. If no display is specified, this command prints the display that has focus.
If the specified display is not currently visible,
FactoryTalk View
prints the display without making it visible. If this command is issued without specifying a display, and no display has focus, nothing happens.Syntax
PrintDisplay <
Me
| display
>
[/U] [/T
<tag>, <tag>, . .
] [/P
<component>
] [/Wait
=tttt
] [/F <File
="pdf
">]
where
<
Me
| display
>
- <Me>prints the current graphic display (the display from which the command is run).
- <display>is a relative or absolute reference to a graphic display. If the file name has a space in it, enclose the name in quotes.
- displayis a relative or absolute reference to the graphic display to be printed. If the file name has a space in it, enclose the name in quotes.
[/U]
initiates an update of tag values in all input fields before starting to print.[/T
<tag>,
]
is the list of tags (separated by commas) to be substituted into the display.[/P
<component>
]
is a relative or absolute reference to a parameter file that contains tag names to be substituted into the display. If the file name has a space in it, enclose the name in quotes.[/Wait=
tttt
]
is the amount of time to wait before starting to print, where tttt
is the time in milliseconds. If you also use the /U parameter, specify enough time to allow for the upload of tag values. FactoryTalk View
[/F <File="
pdf
">]
prints the display to a specified PDF file, where pdf
is the file name with an absolute path. <File="
pdf
">
is optional. You can also specify the file name and location at runtime.Remarks
PrintDisplay
prints the entire runtime display, even if parts are covered by other displays. You can also use the ScreenPrint
command to print an image of whatever shows on the monitor.The
PrintDisplay
command does not necessarily print ActiveX or OLE objects in their runtime state. To ensure that the display is printed with all objects in their current runtime state, use the ScreenPrint
command.This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a FactoryTalk View Studio
or HMI Server.Provide Feedback