PlayWave

Plays the specified wave file.
Syntax
PlayWave
<file>
where
<file>
is the complete path of a wave file including the .WAV extension.
Remarks
This command is run locally on the HMI server,
FactoryTalk View SE
Client, or
FactoryTalk View Studio
that issued it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal