Pause
Specifies a pause between the running two commands. You can use it in macros, from the command line, or as an action for a button.
Syntax
Pause
<seconds>
where
<seconds>
is the number of seconds that will elapse before the next command is run.Remarks
This command is run locally on the HMI server,
FactoryTalk View SE
Client, or FactoryTalk View Studio
that issued it.Provide Feedback