Password

Opens the
Change Password
window for the currently logged-in
FactoryTalk Security
user on the
FactoryTalk View SE
Client.
Remarks
  • This command only supports FactoryTalk users.
  • This command is run only on the
    FactoryTalk View SE
    Client that issued it. It is ignored when it is issued from a
    FactoryTalk View Studio
    or HMI Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal