Logout
Logs the current user out of
FactoryTalk View SE
.When the Logout command is executed, the following occurs:
- All displays are closed (including cached displays).
- The current user's logout macro is executed, and the user is logged out.
- If the FactoryTalk View SE Client is using an activation key, the key is released and made available for other clients to use.
- The login dialog box is presented. A user cannot cancel or close the dialog box and it will continue to be presented until a valid user logs in. However, if this is not what you want, you can configure a Login command in the logout macro.TIP:You can set up the FactoryTalk View SE Client to sign out the current user automatically, after a period of inactivity. For details, clickHelpin the FactoryTalk View SE Client Wizard.
Remarks
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a FactoryTalk View Studio
or HMI Server.Provide Feedback