Help
Displays a Help file.
Syntax
Help [
word
] [/F
file
]
where
[
word
]
is a word you want to search for in the Help file. When you specify a search word, the command will either:- open a list of related topics
- open the Help file if the word uniquely identifies that topic
If no search word is specified, the command opens the default file of:
- the specified Help if/Fis specified
- FactoryTalk View SEHelp if/Fis not specified
[/F
file
]
is the name of a Help file. If no file is specified, the command opens the default Help file of FactoryTalk View SE
.Remarks
- The parameterwordis ignored for HTML files (*.htm or *.html).
- This command is run on theFactoryTalk View SEClient orFactoryTalk View Studiothat issued it. It is ignored when it is issued from an HMI Server.
Provide Feedback