Beep
Runs a wave file to produce a sound from the computer speaker. The sound is a wave file assigned to the Default beep in Window's Control Panel.
Remarks
This command is run locally on the HMI server,
FactoryTalk View SE
Client, or FactoryTalk View Studio
that issued it.Provide Feedback