RecipeProEdit

Use this command to open the RecipePro+ editor and make changes if needed.
Syntax
RecipeProEdit
[
/R
recipename_tag
]
where
[
/R
recipename_tag
] is a relative or absolute reference to a tag that represents the name of the downloaded recipe.
Remarks
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a
FactoryTalk View Studio
or HMI Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal