Example: RecipeProUpload
RecipeProUpload Chocholate
This command reads the tag values from the location specified in the tag set of recipe file
Chocholate
and saves those values to the recipe file.RecipeProUpload $Cookie\Recipename$
Cookie\Recipename
is a tag that represents a recipe file name. At runtime, after you specify a value for the tag, for example, Butter
, this command reads the tag values from the location specified in the tag set of the recipe file Butter
and saves those values to the recipe file.Provide Feedback